Powered by MEAN WELL


MEAN WELL Premium Partner Zone

LEARN MORE

Client Testimonial


ABOUT FEREKS


 

Trading House Fereks LLC is one of the largest manufacturers of LED luminaires in Russia. The company’s production facilities are concentrated at two sites with a total area of over 20,000 m2. Fereks company strives for 90% localization of production. Fereks factory has two “Design and Engineering departments” with highly qualified engineers working in ProEngineer End-to-End Design System. Own lighting laboratory, which includes goniophotometer, allows to measure light distributions of all manufactured products and compose “ies-files” for them.

About 50,000 units are produced under Fereks trademark every month. The range includes over 100 modifications of LED luminaires of various applications. Fereks products have russian and International certificates of conformity. The Company’s Quality Management System meets the requirements of international standard GOST ISO 9001-2011.

Fereks is young and fast-growing Russian LED brand. Largest retailers and factories choose the factory’s products. Fereks illuminates large cities and villages, transport facilities on and under the ground, stadiums and agroindustrial complexes, shopping and business centers. The implemented projects for “IKEA”, “Leroy Merlin”, “Auchan”, etc., illumination of blocks in Kazan-Arena Stadium, Saint-Petersburg Mint of Goznak demonstrate the high level of work of the company. It is no coincidence that Fereks products were chosen for illumination of Innopolis, the youngest and most innovative city of Russia.

By the time of the city opening in june 2015, more than 15,000 luminaires have already been supplied. Fereks street lighting projects are actively developing. In the framework of programmes on modernization of illumination of settlements in Tatarstan and Dagestan, almost 27,000 DKU series street-light luminaires were installed.

The secret of success is in product competitiveness: Fereks luminaires are as good as European analogues, but the price is considerably lower.

For more information, please visit FEREKS website (https://fereks.ru)