Product Notice: LED Driver Product Label Change Notice
Rex.Lin@meanwell.com
In order to provide more eco-friendly manufacturing methods and increase automation productivity, MEAN WELL has changed the following LED driver plastic case models to eliminate using traditional plastic labeling and instead use automated laser engraving placed directly onto the case to reduce the use of plastic compounds and eliminate manual errors. MEAN WELL is doing its part to continuously improve its production processes and reduce its impact on the environment.
This phase in the introduction of laser engraved labeling applies to the following series. If you have any application problems with this change, please contact MEAN WELL's sales representative immediately.
Series | Cut-in lot No. |
Cut-in Date |
NPF-40/D | W2212C | 2022/11/29 |
NPF-60/D | ||
NPF-90/D | ||
NPF-120/D | ||
NPF-200/D | ||
OWA-60E/U | ||
OWA-90E/U | ||
OWA-120E/U | ||
OWA-200E/U | ||
PWM-40(DA/DA2) | W2301A | 2022/12/13 |
PWM-60(DA/DA2/KN/IOT) | ||
PWM-90(DA/DA2) | ||
PWM-120(DA/DA2/KN/IOT) | ||
PWM-200(DA2/KN/IOT) |
Before | After |