Solución para sistema 3+N
What is a 3+N system solution?
3 + N system:“3”means Rack Power, Modular Power and System Power and “N”represents infinite possibilities of MEAN WELL’s product combination and flexibility, for example: a 3+N system can be 20 units of DRP-3200 + CMU2.
MEAN WELL possesses over ten thousand of standardized power supplies and Professional Technical Service Teams deploy worldwide. Through our Sales and Technical Service Teams, MEAN WELL can provide suitable products and solutions to customer’s application or even building a customized 3 + N system for the application.
What the 3+N system solutions MEAN WELL has provided?
Currently, MEAN WELL provides:
1.CMU2 power management system solutions
2.System power solutions
3.High voltage DC LED lighting control solutions
4.IOT wireless LED lighting control solutions
5.DALI smart LED lighting control solutions
6.KNX building automation control solution
7.Burn-in power recycling
MEAN WELL can customize a solution suitable for your applications. If you have questions or inquiries, please feel free to contact us.
What is the difference between 3+N system solutions and previous service methods?
Being a Leading standard power supply Manufacturer with many different Product Lines, MEAN WELL continues developing more intelligent products with complex functionality suitable for new industries. For the general products, such as enclosed type power supplies and LED drivers, our partners and customers are well familiar with and easy to use. However, for those intelligent products such as KNX, MCU controllers, bidirectional power supplies, etc., our partners and customers may struggle to use. MEAN WELL Technical Service team can actively communicate with customers to understand the application requirements and suggest suitable products and solutions to speed the design-in process allowing MEAN WELL to become multi-industry applications solution Provider.
For the 3+N system solutions, where can I find more information and how to contact MEAN WELL Technical Service Team?
We welcome you to download the MEAN WELL app. We provide 3 + N system solutions information from FAQs, Technology News, Technical video and Seminars. If you are a member of the app, you will receive the latest news. The contact information of MEAN WELL Technical Service Team can be found from the link below:
https://expo.meanwell.com.tw/upload/data/C4_tech_team_en.pdf.
Please contact our team member in your region for instant service.
CMU2 power management system solutions?
MEAN WELL’s Intelligent power supplies equip with communication functions, such as PMBus or CAN bus, which can be controlled and monitored remotely and flexible for more applications. However, some may find it’s hard to get started. To reduce the time for the whole construction process in power management, MEAN WELL introduced the CMU2 power management system solutions. CMU2 is not only a fully digitalized master controller but also a Graphic User Interface device that can easily execute monitoring and controlling over intelligent power supplies. Moreover, it can optimize and increase system reliability of your power management system.
Application example:
National Synchrotron Radiation Research Center of Taiwan utilizes a power system built consist of many DRP-3200 to drive solid-state radio frequency power amplifiers, which generates high-frequency energy for boosting electrons to travel at nearly light speed. To match RF power required by the storage ring and best power efficiency, the output voltage of the power system must be adjustable between 42Vdc to 54Vdc modulation range for each operating point with a specific RF power level to achieve the best result. The CMU2 supports CAN bus protocol and is able to control output voltage of up to 48 supplies in a system simultaneously and precisely, which becomes the best solution for the application.
System power solutions?
Power requirement, output voltage levels and functionality vary from different projects and applications. To fulfill such requirements, MEAN WELL proposed a set of flexible and direct solutions called the system power solutions. The system power solution can be assembled and adjusted according to customer application requirement. The power is from 3200W to 128KW, the voltage range is 23.5V - 58.8V. In addition, customers also can choose different cabinet form factors. For more detailed information, please contact our local distributors.
Application example:
Maximum power of MEAN WELL’s system power is up to 128kW, which makes it suitable for laser applications, including CO2 laser, fiber laser and diode laser.
IOT wireless IOT wireless lighting control solutions?
Some of our customers demand a solution that can switch the lights on/off and dim the lights wirelessly by a smart phone or tablet. To satisfy such requirements, MEAN WELL released Bluetooth low energy wireless lighting control solutions. MEAN WELL cooperates with leading technology companies of Casambi, Tuya and Silvair and launched two series of IOT wireless LED drivers, LCM-25/40/60-IOT and PWM-60/120-200-IOT. LCM-IOT series is a constant current mode driver and suitable to directly drive LED lamps; as a constant voltage mode driver, PWM-IOT series is suitable for LED stripes.
Application example:
LCM-25IOT operates with LED lamps for indoor lighting.
DALI smart lighting control solutions?
DALI (Digital Addressable Lighting Interface) is used to provide control over, and communication between, the drivers in a lighting system. DALI also enables lighting control to set up easily and reduce installation cost. As the DALI Association keeps adding new lighting control functions, MEAN WELL not only has DALI 1.0 version digital lighting control products, but also is dedicated to launch new products with the lasted regulation of DALI 2.0. Compared with DALI 1.0, DALI 2.0 adds definitions and functions of the input device and control device, improving and completing the overall DALI lighting system. In the future, LED driver will become a basic lighting device of DALI 2.0 control system.
Application example:
20 sets of LED panel lights with LCM-40DA are installed in an office. There are 3 different areas organized in the office, the designer can assign these 20 lights into 3 different groups through the DALI controller. It is easy to set up and easy to change in the future.
MEAN WELL's DALI 1.0 products:
LCM-25DA/40DA/60DA
LCM-40UDA/60UDA
ELG-75CDA/100CDA/150CDA/200CDA/240CDA
ELG-75DA/100DA/150DA/200DA/240DA
HLG-320-CDA
HBG-100DA/160DA/200DA/240DA
HBC-100PDA/160PDA
HVGC-480ADA/650DA
LDC-35DA/55DA/80DA
PWM-60DA/90DA/120DA
DAP-04
LDD-H-DA
MEAN WELL's DALI 2.0 products:
LCM-25DA2/40DA2/60DA2
PWM-60DA2/90DA2/120DA2/200DA2
XLG-50/75/100/150/200/240/320-DA2
ELGC-300-L/M/H-ADA
HBGC-300-L/M/H-ADA
HVGC-1000-L/M/H-DA
LDC-55DA2
DLC-02
KNX building automation control solutions?
KNX FAQ https://building.meanwell.com/qa.aspx?c=10
KNX SOLUTIONS https://www.meanwell.com/KNX/BA/en/index.html
KNX is the world standard for residential and building control, offering many new products for visualization and building automation systems on the market.
MEAN WELL has been promoting KNX building automation control technology for a green and sustainable society and has continuously launched KNX related products that meet International Standards, such as KAA-8R universal switch actuator and KAA-4R4V dimming actuator, depending on the application they are suitable with MEAN WELL various power supplies and LED driver. Based on the KNX architecture, KNX system engineers can easily program through the ETS system as needed during planning or use. So far, MEAN WELL continues to improve product integrity to meet the needs of end customers and system operators.
Application example:
The Blinder system is a major part of the intelligent building control. To meet the application demand, MEAN WELL developed KNX bus power supply KNX-20E and KNX-40E to provide KNX equipment power, while KNX logic switch actuator has KNX-KAA-8R. KAA-8R can be applied with a light sensor and electrical blinder or curtains to control the blinder system.
MEAN WELL's KNX products:
LCM-25KN/40KN/60KN
PWM-60KN/120KN/200KN
XLC-25/40/60KN
KAA-8R(-10)
KAA-4R4V(-10)
KDA-64
KNX-20E-640/40E-1280D
DLC-02KN
Burn-in power recycling?
Any manufacturer that produces electronic products and equipment must undergo burn-in and aging tests in the production process. However, the burn-in process consumes a lot of electricity. To improve the problem of power consumption, MEAN WELL uses our self-developed energy recovery power supply combined with the power monitoring system (CMU2) to recycle the power consumed during the burn-in test, which can reduce energy consumption by more than 70%, up to 90%.
Please click the link below for detail and case study.
https://expo.meanwell.com/aboutRangeC3.aspx?i=64